Multistate Alarm Attributes - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Multistate Alarm Extension contains attributes common to Metasys system objects. For details, see the Common Object Attributes.

The following table lists the attributes specific to the Multistate Alarm extension. Click the attribute name in the table for a description of the attribute.

Note: In the Notes column, letters indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable.
Table 1. Multistate Alarm Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Alarm Ack Pending

 

False

Ack not pending, Ack pending

Alarm Ack Required

C,W

False

Ack not required, Ack required

Alarm Date

     

Alarm Message Text

C,N,W

   

Alarm Priority

C,W

70

Alarm Time

     

Alarm Values

C,W

   

Capture Changes

 

False

 

Command Reference

C,W

   

For more information on how this attribute works with regard to AO/BO point feedback, see AO/BO Feedback.

Date

     

Indicates the date of the last reported condition.

Event Enable

C,W

True

 

Graphic

C,N,W

Null

Object Type = Graphic

Do not set the Graphic attribute for an alarm extension to an aliased graphic. Aliased graphics do not display properly when displayed from the Alarms Window or Event Viewer.

Graphic Alias

C,W

 

Maximum 256 characters

Input

   

Derived from Input Reference, the object to which the Multistate Alarm extension has been attached.

Input Reference

C

   

Normal Ack Pending

 

False

Ack not pending, Ack pending

Normal Ack Required

C,W

False

Ack not required, Ack required

Normal Date

     

Normal Priority

C,W

200

Normal Time

     

Normal State

C,W

State 0

Derived from Input Reference, the object to which the Multistate Alarm extension has been attached.

Present Value

D,R

Normal

Normal, Alarm, Hold

Reference Delay Time

C,W

0

0–65,535 seconds

When a Binary Output Object (BO) (supply fan command) is commanded On, the Normal State for the associated Binary Input Object (BI) (supply fan status) alarm extension is also On. After the Reference Delay Time, the current state of the BI is compared to the Normal State. If the BI is still Off, an alarm is detected. The Reference Delay Time is also used when the BO is commanded Off.

Specifies the feedback delay in seconds. The purpose of the Reference Delay Time is to allow time for equipment to start or stop before the status is compared to the command.

Reference Delay Timer Active

 

False

 

Reliability

 

Input Unreliable

Uses Reliability (Set 503).

Report Delay

C,W

0

0–65,535 seconds

Report Delay Active

C,W

False

 

Status

     

Disabled: Enabled attribute value is False.

Unreliable: Reliability attribute is not reliable.

Normal: Expected operating condition.

Time