Cooling/Heating Setpoint Mode - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Using the Cooling/Heating Setpoint Mode, the object calculates up to seven different statuses based on the Cooling Setpoint Reference and the Heating Setpoint Reference. You can also define an optional Occupancy Reference to suppress the status of the extension and display an unoccupied status indication color unless there is a high or low alarm.

Figure 1. Cooling/Heating Setpoint Mode