Analog Alarm Attributes - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Analog Alarm Extension contains attributes common to Metasys system objects. For details, see Common Object Attributes.

The following table lists the attributes specific to the Analog Alarm extension. The list of Attribute names are displayed in the Focus Window of the Site Management Portal view of the Alarm Extension. Click the attribute name in the table for a description of the attribute.

Notes:
  • In the Notes column, letters indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable.
  • In the SUM (Tailored Summary Pick) column, attributes marked with an X can be used in the Tailored Summary User View. See the Defining User Views with Summary Definitions section for information about recommended groupings of Summary Definitions in a Tailored Summary.
  • In the MOD (Global Modify) column, attributes marked with an X can be mass edited from a Tailored Summary or Global Search Results.
  • In the SCT (SCT Configuration Attribute) column, attributes marked with an X are viewable in the SCT Alarm Extension Focus Window.
Table 1. Analog Alarm Attributes (SUM=Tailored Summary; MOD=Global Modify; SCT=SCT Configurable)

Attribute Name

Notes

Initial Value

Values/ Options/Range

Description

SUM

MOD

SCT

Alarm Ack Pending

 

False

Ack not pending, Ack pending

X    

Alarm Ack Required

C,W

False

Ack not required, Ack required

X X X

Alarm Date

      X    

Alarm Message Text

C,N,W

    X X X

Alarm Priority

C,W

70

  X X X
Alarm Time       X    

Cooling Setpoint

C,N,W

Null

       

Cooling Setpoint Reference

C,W

Null

 

When specified, indicates the Above Setpoint limit. You must define both the Cooling Setpoint Reference and Heating Setpoint Reference, or leave both blank. If the Cooling Setpoint Reference is defined, the High Warning Offset is added to the Cooling Setpoint Reference value to calculate the High Warning Limit.

X X X

Date

           

Description

C,W

 

Maximum 40 characters before Release 8.0. Maximum 64 characters at Release 8.0 and later.

Identifies the alarm extension in detail.

    X

Differential

C,W

0.00

Positive value

When the Cooling Setpoint and the Heating Setpoint are configured, the Differential specifies:

  • The deadband range for transitions to the Above and Below Setpoint states.
  • The deadband range for transitions from Above and Below Setpoint states to return to a Normal state. In this case, half of the value specified for the Differential is used. This allows the value to return to normal in cases where the control algorithm controls to a value close to the setpoint, but may not achieve or cross the setpoint.
X X X

Enabled

W

True

 

Indicates whether the alarm extension is enabled.

    X

Error Log

     

Indicates the reliability of the following references:

  • Input Ref Status
  • Warning Ref Status
  • Setpoint Ref Status
  • Cooling Setpoint Ref Status
  • Heating Setpoint Ref Status
  • Occupancy Ref Status

If a reference is not defined, the value will be No Input.

     

Event Enable

C,W

True

    X X

Graphic

C,N,W

Null

Object Type = Graphic

Do not set the Graphic attribute for an alarm extension to an aliased graphic. Aliased graphics do not display properly when displayed from the Alarms Window or Event Viewer.

  X X

Graphic Alias

C,W

 

Maximum 256 characters

  X X

Heating Setpoint

C,N,W

Null

 

You can either define the Cooling Setpoint and Low Alarm Limit or the Setpoint Reference.

     

Heating Setpoint Reference

C,W

Null

  X X X

High Alarm Limit

C,N,W

         

High Alarm Limit

 

Null

  X X X

High Warning Offset

C,N,W

 

Positive value

X X X

Input

           

Input Reference

C

         

Item Reference

           

Low Alarm Limit

C,N,W

    X X X

Low Warning Offset

C,N,W

 

Positive value

X X X

Name

C,W

 

Maximum 400 characters

Name of the alarm extension attribute.

  X X

Normal Ack Pending

 

False

Ack not pending, Ack pending

X    

Normal Ack Required

C,W

False

Ack not required, Ack required

X X X

Normal Date

      X    

Normal Priority

C,W

200

  X X X

Normal Time

      X    

Object Identifier

     

Specifies an internal identifier assigned to the alarm extension.

    X

Object Name

     

Identifies the name of the object associated with the alarm extension.

     

Object Type

 

Analog Alarm

 

Identifies the type of alarm extension.

    X

Occupancy Reference

C,W

Null

  X X X

Present Value

D,R

Normal

Normal,

Low Warning,

High Warning,

Low Alarm,

High Alarm

     

Reference Delay Time

C,W

0

0 to 65,535 seconds

X X X

Reference Delay Timer Active

 

False

  X   X

Reliability

 

Input Un-reliable

Uses Reliability (Set 503).

     

Report Delay

C,W

0

0 to 65,535 seconds

X X X

Report Delay Active

C,W

False

  X    

Setpoint Reference

C,W

Null

  X X X

Status

     
  • Disabled: Enabled attribute value is False.
  • Unreliable: Reliability attribute is not reliable.
  • Normal: Expected operating condition.
     

Time

           

Version

     

Specifies the version number for the alarm extension.

     

Unoccupied State

C,W

1

Set re-directed to Unoccupied_Set Attribute

X X X

Unoccupied State Set

           

Username is BACnet Object Name

 

False

 

Controls whether the object’s User Name attribute is also the Object Name attribute. The Object Name attribute is not writable, so the only way to change the Object Name attribute is to edit the User Name attribute and set the User Name Is BACnet Obj Name attribute to True.

    X

Warning Ack Pending

 

False

Ack not pending, Ack pending

X    

Warning Ack Required

C,W

False

Ack not required, Ack required

X X X

Warning Date

      X    

Warning Priority

C,W

120

  X X X

Warning Reference

C,W

0.00

  X X X

Warning Time

      X