Alarm Extensions - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Alarm extensions monitor an attribute of an object and send alarms using the Alarm and Event Management feature. There are two types of alarm extensions, Analog Alarm and Multistate Alarm. Use the Analog Alarm extension to monitor attributes with real values. Use the Multistate Alarm extension to monitor attributes with True or False, or Multistate data types.

For general information on Metasys system objects, see the Object Help section.