Site Discovery - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English
Notes:
  • To ensure Site Discovery performance, the local application (Controller Application File/CAF file) for any field controller is not uploaded during the process.
  • You can use the Manage Archive/Upload function after the initial site discovery of devices to upload and add the CAF files into the archive.
  • Discovering objects within a device that contains a large number of objects can require several minutes to complete.
  • The SCT device order may differ from the order displayed in the ADS/ADX until you upload the Site Director. If the SCT device order remains unordered after you upload the Site Director, use the All Items Organizer to manually specify the order of devices.

After Site Discovery, immediately perform an upload of the engine to ensure the archive database is current with the online database.