Import Integration - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Menu Selection: Action > Import Integration

This command is only available when an Integration under an engine is selected in the All Items tree. After adding an Integration, you can select the integration in the navigation tree and use this menu selection to add existing devices and points under the integration.