Import Definition - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Menu Selection: Action > Import Definition

Imports the pre-built summary definition that is stored on the computer and is only available when the Summary Definitions folder is selected in the All Items tree. After importing a definition, the imported Summary Definitions appear in the Summary Definitions folder in the All Items tree.

Note: You also can import Summary Definitions that were previously exported.