Action Menu - Feature Specific - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The following table describes the different menu items that appear in the Action menu based on the active panel or feature displayed in the selected display panel. Click each active panel or feature for a description. For more information on the modes of operation, see Modes.

Note: The Refresh, Refresh Current Tab, and Refresh All Tabs menu items appear in the Action menu for all other features or active panels.
Table 1. Action Menu - Feature Specific

Active Panel/Feature

Content

Event Viewer

  • Refresh
  • Add Annotation (available on the only.)
  • View Annotations (available on the only.)
  • Ack
  • Discard

Audit Viewer

  • Refresh
  • Add Annotation (available on the only.)
  • View Annotations (available on the only.)
  • Clear Audit Log

ActionQ

 

Tailored Summary Viewer

The menu options available are item-specific (that is, they depend on the type of item selected in the Summary Definitions and Key Data tables).

  • Command
  • Modify
  • Add Annotation (available on the only.)
  • View Annotations (available on the only.)
  • Show Extensions
  • Remove From Site (available for a network engine only).
  • Import Integration (available for a Tailored Summary with trunk/integration data. For example, trunk diagnostics).

Global Search

  • Refresh

Change Results Viewer

No Action menu options for this feature.