How do I transfer logic files from a field controller to SCT Pro (upload)? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 15.0
SCT Pro Help
- Product
- Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
- Document number
- LIT-12013035
- Version
- 15.0
- Revision date
- 2022-05-20
Procedure
-
Open an archive.
-
In the Network Tree pane, select the devices to include
in the upload.
-
Click Actions, and then click Upload
(Transfer To Archive).
-
Select a connection method and then complete one of the following steps:
- To connect through the Site Director, enter the credentials for the Site
Director, and then click Authenticate.
- To connect through individual network engines, enter the credentials
for a network engine, and then click
Authenticate. The padlock icon shows as unlocked for
all devices where the logon is successful. If you fail to log on to a
device, select the check box for that device, enter the correct logon
information, then click Authenticate.
- To connect through a direct Ethernet connection, verify that you are
connected to the same subnet as the IP controller, enter the UDP port of the
device, and then select the appropriate network interface.
- To connect through a MAP 4.2+ or BACnet Router, enter the IP address and
UDP port of the router, enter the network number of the MS/TP trunk, and
then select the appropriate network interface.
-
Click Continue.
-
Review the summary screen. If you want to change any of the default settings,
see How do I change the upload or download settings?
-
Click Transfer Now. To confirm that the download
completes successfully, view the corresponding entry in the Action
Queue.