How do I transfer logic files from SCT Pro to a field controller (download)? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 15.0
SCT Pro Help
- Product
- Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
- Document type
- User Guide
- Document number
- LIT-12013035
- Version
- 15.0
- Revision date
- 2022-05-20
Procedure
-
Open an archive.
-
In the Network Tree pane,
select the devices to include in the download.
-
Click Actions, and then
click Download (Transfer To Device).
-
Select a connection method and then complete one of the
following steps:
- To connect through the Site Director, enter the
credentials for the Site Director, and then click Authenticate.
- To connect through individual network engines, enter the
credentials for a network engine, and then click Authenticate. The padlock icon shows as unlocked for all
devices where the logon is successful. If you fail to log on to a device,
select the check box for that device, enter the correct logon information,
and then click Authenticate.
- To connect through a direct Ethernet connection, verify
that you are connected to the same subnet as the IP controller, enter the
UDP port of the device, and then select the appropriate network
interface.
- To connect through a MAP 4.2+ or BACnet Router, enter
the IP address and UDP port of the router, enter the network number of the
MS/TP trunk, and then select the appropriate network interface.
-
Click Continue.
-
Review the summary screen. If you want to change the default
download settings, see How do I change the upload or download settings? For example, you can choose how
CAF files are activated for controllers. For more information see How do I control the execution of controller logic as part of a download?
-
Depending on your choices, click Transfer Now or Schedule
Transfer. To confirm that the download completes successfully,
view the corresponding entry in the Action
Queue.