To access SCT, use one of the following methods:
- If you have Launcher installed on the computer that you are using, start Launcher to access SCT. Refer to the Launcher section in SCT: System Configuration Tool Help (LIT-12011964).
- If Launcher is not installed on the
computer that you are using, complete the following steps:
- In the upper-right of the SCT Pro window, click your account name, and then click Logout.
- In the SCT Pro logon page, click Looking for Launcher?
- Download and launch the Launcher application. Refer to the Launcher section in SCT: System Configuration Tool Help (LIT-12011964), the Launcher Installation Instructions (LIT-12011783), or the Launcher Help (LIT-12011742).