How can I access the full features of SCT through SCT Pro? - Metasys - LIT-12013035 - Software Application - SCT Pro - 15.0

SCT Pro Help

Brand
Metasys
Product name
SCT Pro
Document type
User Guide
Document number
LIT-12013035
Version
15.0
Revision date
2022-05-20
Language
English

To access SCT, use one of the following methods:

  • If you have Launcher installed on the computer that you are using, start Launcher to access SCT. Refer to the Launcher section in SCT: System Configuration Tool Help (LIT-12011964).
  • If Launcher is not installed on the computer that you are using, complete the following steps:
    1. In the upper-right of the SCT Pro window, click your account name, and then click Logout.
    2. In the SCT Pro logon page, click Looking for Launcher?
    3. Download and launch the Launcher application. Refer to the Launcher section in SCT: System Configuration Tool Help (LIT-12011964), the Launcher Installation Instructions (LIT-12011783), or the Launcher Help (LIT-12011742).