Before you begin
- Log on to SCT Pro.
- Ensure that you have the required engine images on your laptop.
- Create an archive that has an engine that can be upgraded.
- Before you upload the engine, open the engine under Details and ensure that the Model Name attributes is empty.
About this task
Important: At Metasys Release 10.1 or later the Advanced Security Enabled
attribute is set to
True
by default for a site.
When the value is set to True
, a site director at
Metasys Release 10.0 or later discards all communication attempts from network
engines at Metasys Release 9.0.7 or earlier. For more information, see How does the Advanced Security Enabled attribute affect my site?
Note: You can use the Upgrade Device feature in SCT Pro to perform all of
the tasks required to upgrade a network engine. However, if you use the Upgrade Device feature to upgrade a server then you
must manually perform additional tasks on the server.