How do I factory reset a device? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 15.0

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document type
User Guide
Document number
LIT-12013035
Version
15.0
Revision date
2022-05-20

To factory reset a device, perform a reflash operation, but re-apply the same firmware version. In Device Discovery, the Device Version column displays the current firmware version of devices, as shown in Figure 1. Before you start the reflash operation, note the Device Version of the device so that you can re-apply the same version. For more information about how to perform a reflash operation, see Reflashing a device.

Figure 1. Example results in Device Discovery