How do I set the number of automatic backup files to keep? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 15.0

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document type
User Guide
Document number
LIT-12013035
Version
15.0
Revision date
2022-05-20

About this task

If you schedule automatic backups, only a limited number of backup files are retained on the SCT computer. Once you reach the limit of archive backups, the new backup overwrites the oldest saved backup. To change the number of backup files retained, complete the following steps:

Procedure

  1. Click on your account name in the upper-right corner of the SCT Pro window, then click Settings.
  2. On the Settings page, click System Settings.
  3. In the Backup Revisions field, enter the number of backups that you want to retain.