How do I restore an archive from a downloaded file? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 15.0

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document type
User Guide
Document number
LIT-12013035
Version
15.0
Revision date
2022-05-20

About this task

To watch a video that demonstrates this feature, refer to uLearn: Restore an Archive using SCT Pro.

To restore an archive database from either a Database backup or Export File that you have downloaded, complete the following steps:

Procedure

  1. In the Utilities pane, click Restore. The Archive Restore window appears.
  2. Click Choose File, browse to the .backup or .DbExport file, and click Open.
  3. Enter a new Archive Name.
  4. Optional: In the Note field, enter a description for future reference.
  5. Optional: If the certificates in the archive are password protected, enter the password in the password field.
  6. Click Restore. The file uploads to SCT Pro. To confirm that the restore task completes successfully, view the corresponding entry in the Action Queue.