How do I license SCT Pro? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 15.0

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document number
LIT-12013035
Version
15.0
Revision date
2022-05-20

SCT and SCT Pro software require license activation from SCT Release 13.0 and SCT Pro Release 10.0. SCT Pro is included in the license of SCT, and is not licensed as an individual product. Activate your license through the Software Manager. For more information on licensing, refer to the Software Manager Help (LIT-12012389).

If a license for SCT is not active, or the license expires, then a message displays on the SCT Pro logon window. You cannot log on to SCT Pro when there is no active license. To view the number of days remaining on your license, after you log on, click on your account name in the upper-right corner of SCT Pro, and then click About.

If there are less than two weeks remaining on your license, a message displays on the SCT Pro logon window showing the number of days remaining. Click Continue to log on.