Accessing SCT Pro - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 15.0

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document type
User Guide
Document number
LIT-12013035
Version
15.0
Revision date
2022-05-20

Procedure

  1. In a web browser, navigate to https://[Host Name or IP address]/SCTPro, where [Host Name or IP address] is replaced with the Host Name or IP address of the SCT computer. If you are browsing to SCT Pro on the SCT computer, then use https://localhost/SCTPro.
    Note: SCT Pro does not support Internet Explorer.
    Note: When browsing to SCT Pro, your web browser displays a security certificate warning if your SCT Pro site does not have a trusted security certificate. For more information, see Why do I see a security warning when accessing SCT Pro?
  2. In the SCT logon window, enter your credentials. Click Login.
    Note: A note displays above the Username field if an update is available for SCT Pro. Clicking this link opens information about the update. You must use the software manager to update SCT Pro.