What is the difference between upload and download? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 10.2

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document number
LIT-12013035
Version
10.2
Revision date
2020-01-21

The terms upload and download both relate to the transfer of archive information between SCT or SCT Pro, and devices, such as Metasys servers and network engines. Download is the transfer from an SCT or SCT Pro archive to devices. Upload is the transfer from devices to SCT or SCT Pro archive.

If you initiate an upload or a download, SCT Pro determines whether the selected devices are Metasys servers, network engines, or field controllers, and presents the appropriate interface for you to complete the task.