How do I transfer logic files from SCT Pro to a field controller (download)? - Metasys - LIT-12013035 - Software Application - SCT Pro - 10.2

SCT Pro Help

Brand
Metasys
Product name
SCT Pro
Document type
User Guide
Document number
LIT-12013035
Version
10.2
Revision date
2020-01-21
Language
English

Procedure

  1. Open an archive.
  2. In the Network Tree pane, select the devices to include in the download.
  3. Click Actions, and then click Download (Transfer To Device).
  4. Select a connection method and then complete one of the following steps:
    • To connect through the Site Director, enter the credentials for the Site Director, and then click Authenticate.
    • To connect through individual network engines, enter the credentials for a network engine, and then click Authenticate. The padlock icon shows as unlocked for all devices where the logon is successful. If you fail to log on to a device, select the check box for that device, enter the correct logon information, and then click Authenticate.
    • To connect through a direct Ethernet connection, verify that you are connected to the same subnet as the IP controller, enter the UDP port of the device, and then select the appropriate network interface.
    • To connect through a MAP 4.2+ or BACnet Router, enter the IP address and UDP port of the router, enter the network number of the MS/TP trunk, and then select the appropriate network interface.
  5. Click Continue.
  6. Review the summary screen. If you want to change the default download settings, see How do I change the upload or download settings?. For example, you can choose how CAF files are activated for controllers. For more information see How do I control the execution of controller logic as part of a download?.
  7. Depending on your choices, click Transfer Now or Schedule Transfer. To confirm that the download completes successfully, view the corresponding entry in the Action Queue.