How do I transfer an archive from SCT Pro to a Metasys server or network engine (download)? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 10.2
SCT Pro Help
- Product
- Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
- Document number
- LIT-12013035
- Version
- 10.2
- Revision date
- 2020-01-21
Procedure
-
Open an archive.
-
In the Network Tree pane, select the devices to include
in the download.
-
Click Actions, then click Download (Transfer
to Device).
-
Click Site Director to communicate through the Site
Director, or click Individual Devices to communicate with
each device individually.
-
Enter a user name and password, and click Authenticate
to log on. The padlock icon shows as unlocked for all devices where the logon is
successful. If you fail to log on to a device, select the check box for that
device, enter the correct logon information, and then click
Authenticate.
Figure 1. Selected Devices list, showing successful logon (top) and
unsuccessful logon (bottom)
-
Click Continue.
-
Review the summary screen. If you want to change any of the default settings,
see How do I change the upload or download settings?.
For example, you can choose how to activate downloaded
files on network engines that support background file transfer. For more
information, see How do I control the activation of network engines as part of a download?.
-
Depending on your choices, click Transfer Now or Schedule
Transfer. To confirm that the download completes successfully,
view the corresponding entry in the Action
Queue.