How do I create a new archive? - Metasys - LIT-12013035 - Software Application - SCT Pro - 10.2

SCT Pro Help

Brand
Metasys
Product name
SCT Pro
Document type
User Guide
Document number
LIT-12013035
Version
10.2
Revision date
2020-01-21
Language
English

About this task

You can use SCT Pro to perform an upload from a Site Director, and use that information to create a new archive.

Procedure

  1. On the SCT Pro Dashboard, in the Archives pane, click New.
  2. In the Archive Name field, enter a unique name for the archive.
  3. In the Site Director field, enter the name of the Site Director.
  4. Optional: To use the IP address of the Site Director to establish a connection, below the Site Director field, click Change. In the Host field, enter the IP address of the Site Director, and then click Apply.
  5. In the Security section, enter credentials for the Site Director, and then click Authenticate. If authentication is successful, the padlock icon shows as unlocked and the message Authenticated appears.
  6. Optional: To upload device objects from the Site Director and all child network engines, select Full Device Details.
  7. Click Create New Archive. To confirm that the task completes successfully, view the corresponding entry in the Action Queue.