How can I access the full features of SCT through SCT Pro? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 10.2

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document type
User Guide
Document number
LIT-12013035
Version
10.2
Revision date
2020-01-21

To access SCT, use one of the following methods:

  • If you have Launcher installed on the computer that you are using, start Launcher to access SCT. Refer to the Launcher section in Metasys SCT Help (LIT-12011964).
  • If Launcher is not installed on the computer that you are using, complete the following steps:
    1. In the upper-right of the SCT Pro window, click your account name, and then click Logout.
    2. In the SCT Pro logon page, click Looking for Launcher?
    3. Download and launch the Launcher application. Refer to the Launcher section in Metasys SCT Help (LIT-12011964), the Launcher Installation Instructions (LIT-12011783), or the Launcher Help (LIT-12011742).