How do I issue commands to a controller? - Metasys - LIT-12013035 - Software Application - SCT Pro - 10.2

SCT Pro Help

Brand
Metasys
Product name
SCT Pro
Document type
User Guide
Document number
LIT-12013035
Version
10.2
Revision date
2020-01-21
Language
English

Procedure

  1. Open an archive.
  2. Select the controllers or trunk to receive the command.
  3. Click Actions, and then click Command.
  4. In the Commands section, select one of the following options:
    • Select Activate Pending Files to command controllers to activate CAF files that you downloaded but did not activate.
    • Select Enable Logic to enable the logic on the controllers.
    • Select Disable Logic to disable the logic on the controllers.
  5. Select a connection method and then complete one of the following steps:
    • To connect through the Site Director, enter the credentials for the Site Director, and then click Authenticate.
    • To connect through individual network engines, enter the credentials for a network engine, and then click Authenticate. The padlock icon shows as unlocked for all devices where the logon is successful. If you fail to log on to a device, select the check box for that device, enter the correct logon information, and then click Authenticate.
    • To connect through a direct Ethernet connection, verify that you are connected to the same subnet as the IP controller, enter the UDP port of the device, and then select the appropriate network interface.
    • To connect through a MAP 4.2+ or BACnet Router, enter the IP address and UDP port of the router, enter the network number of the MS/TP trunk, and then select the appropriate network interface.
  6. Click Continue. To confirm that the task completes successfully, view the corresponding entry in the Action Queue.