How do I schedule a backup to run automatically? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 10.2

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document number
LIT-12013035
Version
10.2
Revision date
2020-01-21

About this task

You can schedule the creation of a backup at a specific time and date, or on a recurring basis. To schedule a backup, complete the following steps:

Procedure

  1. From the Dashboard, select the archive to backup on a schedule.
  2. In the Backups pane, click New.
  3. In the New Backup window, click Schedule For Later.
  4. In the Create Schedule section, select how frequently to perform the backup.
  5. In the backup format section, select one of the following options:
    1. Select Database to create an SQL dependent backup file (.backup).
    2. Select Export File to create an SQL independent XML file (.DbExport).
  6. Click Create Backup.