SCT Pro is the next generation of interface for SCT. It provides significantly streamlined workflows, and greatly simplifies tasks that were previously time consuming or cumbersome. For example, you can use SCT Pro to maintain healthy backup practices for a site, including the creation of backups automatically on a recurring schedule. SCT Pro does not include the full range of features that are available in SCT, but we add new features in each release; and SCT remains available for the tasks that SCT Pro does not yet support.
To watch a video that provides an overview of SCT Pro, refer to uLearn: Welcome to SCT Pro.