How do I access SCT Pro? - Metasys - LIT-12013035 - Software Application - SCT Pro System Configuration Tool - 10.2

SCT Pro Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT Pro System Configuration Tool
Document number
LIT-12013035
Version
10.2
Revision date
2020-01-21

Access SCT Pro using one of the following methods:

  • In a web browser, navigate to https://[Host Name or IP address]/SCTPro, where [Host Name or IP address] is replaced with the Host Name or IP address of the SCT computer. If you are browsing to SCT Pro on the SCT computer, then use https://localhost/SCTPro.
  • In the SCT logon window, click SCT Pro.
  • In SCT, from the SCT Pro menu, click Dashboards.

When browsing to SCT Pro, your web browser displays a security certificate warning if your SCT Pro site does not have a trusted security certificate. For more information, see Why do I see a security warning when accessing SCT Pro?