SCT installation and upgrade overview - Metasys - LIT-12012067 - Software Application - SCT System Configuration Tool - 16.0

SCT Installation and Upgrade Instructions

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12012067
Version
16.0
Revision date
2023-10-02

The Windows operating system that you want to use for SCT software must have the correct components installed. SCT software does not install or function properly if any of these components are missing. The SCT setup installs many of these prerequisites, but make sure you carefully review the software requirements before installation. Follow the steps outlined in the Detailed procedures section to ensure that SCT successfully installs.

You cannot install SCT Release 15.0 and later on a computer with a Metasys server that is at Metasys Release 11.0 or earlier. Metasys servers include the ADS, ADX, and ADS-Lite. Do not install the SCT software on an OAS server. Consider the following installation rules:

  • SCT software and Trunk Utility features require license activation at Release 13.0 or later. Use the Software Manager to license SCT, device, and field controller packages. Install the software manager through the SCT installation wizard. For more information on software licensing, refer to the Software Manager Help (LIT-12012389) .
  • You must uninstall any older stand-alone releases of the NAE/NIE Update Tool (NUT) before you use the SCT setup to install SCT Release 13.0 and later.
  • You must uninstall SCT Release 13.0 or earlier software before installing SCT Release 16.0.
  • You must apply any new OS or SQL service pack after you remove an older release of the SCT, but before you install a new release of SCT.
  • Do not install SCT and Metasys Server software on the same computer if more than 100 network engines are to report to one ADX. If you have more than 100 engines on the site, install SCT on a separate computer.
  • You can use SCT to manage devices from Metasys Release 5.2 or later. SCT Release 7.0 and later no longer require the Site Director to be of an equivalent release version as the tool.
  • Install SCT on a stand-alone computer when you use it with a split ADX system. Do not install SCT on the same computer as the web/application server or database server of a split ADX system.