Launching the SCT user interface - Metasys - LIT-12012067 - Software Application - SCT System Configuration Tool - 16.0

SCT Installation and Upgrade Instructions

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12012067
Version
16.0
Revision date
2023-10-02

About this task

To launch the SCT UI, do one of the following:

  • On the SCT computer, go to Start > Programs > Johnson Controls > Launcher. Click the Launcher icon on the Desktop. Follow the steps in Launcher Help (LIT-12011742) to add the SCT computer's profile to the Launcher.
  • On another computer on the same network as the SCT computer, first uninstall any older version of the Launcher software from the client. Then, browse to https://[Host name or address]/SCT/ where [name or address] is the computer name or IP address of the computer on which the SCT is installed.

    When you browse to the SCT computer from a client for the first time, the Launcher Download screen appears. Start the SCT UI using the Launcher downloaded JRE. Click Full Launcher Installer to retrieve the user interface files from the SCT computer, then run the Launcher installation file. For details, refer to the Launcher Installation Instructions (LIT-12011783).

    After you install the Launcher to your local hard disk, double-click its icon on the computer desktop. The Main Screen of the Launcher appears. Add a profile for the SCT computer. For details, refer to Launcher Help (LIT-12011742) .

    Figure 1. Launcher main screen

    After you add the SCT profile, select it from the profile list under the SCT tab and click Launch. The Metasys System Configuration Tool logon screen appears.

    Log on with the MetasysSysAgent user and default password. To obtain the default password, contact your local Johnson Controls representative. The Change Password screen appears for the MetasysSysAgent user. Type the old password, then type a new password twice. The new password must follow the rules listed in the Change Password screen. To look up words that cannot be passwords, click View Blocked Words List.

    Click OK. When Successfully changed the password appears in the Change Password dialog box, click OK. The Terms and Conditions dialog box appears. Click Accept. If no archive databases exist on the system, the New Archive Wizard user interface screen appears (Figure 2).

    Figure 2. New archive wizard screen

    To learn how to create a new archive and use all the features of SCT, refer to SCT: System Configuration Tool Help (LIT-12011964). If you see any error messages while logging into and using SCT, see Troubleshooting.