SCT software one-click installation - Metasys - LIT-12012067 - Software Application - SCT System Configuration Tool - 16.0

SCT Installation and Upgrade Instructions

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12012067
Version
16.0
Revision date
2023-10-02

About this task

Note: Installation of the prerequisite software for SCT occurs before the installation of the SCT software. If not detected, the SCT download manager also installs .NET Framework 4.7.2 or later.

Procedure

  1. Obtain the SCT installation file from the License Portal.
  2. Right click SystemConfigurationTool_16.0.exe and select Run as administrator.
  3. On the System Configuration Tool Setup window, click Install.
  4. If the message Install will continue after restart appears, click Restart Now to restart your computer. The installation continues after you restart the computer and log on to Windows.
  5. Click Finish.
    Note: Before you can use all features within SCT, you must license both SCT as well as install and license SCT packages. See Licensing SCT and importing and licensing packages for SCT for these steps.