Note: If you are uninstalling the SCT to install an earlier release, see
Uninstalling SCT to install an earlier release of SCT
for more information.
Important: You need to uninstall
SCT Release 11.0 or earlier software before you can use the System
Configuration Tool Setup to install the latest release of SCT.
Important: If you receive error messages when you uninstall SCT software, you may have problems reinstalling it. Diagnose these problems before you attempt to reinstall the software.
Important: The security database
for the SCT application is not available after uninstalling and
reinstalling the software when you select the Remove Databases
option. Before uninstalling the SCT software, document the existing
list of SCT users and after reinstalling the software manually add
the users to the database again.