Security certificate warnings - Metasys - LIT-12012067 - Software Application - SCT System Configuration Tool - 15.0

SCT Installation and Upgrade Instructions

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12012067
Version
15.0
Revision date
2022-06-29
Note: Ensure that your web browser has cookies enabled before browsing to JCT or SCT Pro.

When browsing to JCT or SCT Pro, your web browser displays a security certificate warning if your JCT and SCT Pro site does not have a trusted security certificate. If you enter localhost as the server name, your web browser displays a security certificate warning even if you install a trusted security certificate.

If you see a security certificate warning, complete the following steps to browse to JCT or SCT Pro:
  • For Google® Chrome™ browsers:
    1. Tap or click Advanced.
    2. Tap or click Proceed to [name or IP Address], where [name or IP Address] is the computer name or IP address of the computer on which the SCT is installed. The JCT or SCT Pro logon screen appears.
  • For Microsoft Edge, tap or click Advanced, then click Continue to localhost (not recommended). The JCT or SCT Pro logon screen appears.
  • For Apple® Safari®: tap or click Continue in the Cannot Verify Server Identity window. The JCT or SCT Pro logon screen appears.
Note: JCT does not support autofill functionality for the username or password fields.

For more information about implementing security certificates for the Metasys UI or the SCT Pro sites, refer to the Appendix: Security Certificate Implementation section of the Network and IT Guidance Technical Bulletin (LIT-12011279) .