Use the following table to resolve issues that may occur during installation. If the SCT ceases to function correctly, and you cannot find a solution in the following table, uninstall and reinstall the SCT. Under normal circumstances the SCT software installer sets up all of the required components.
|
Problem |
Solution |
|
|---|---|---|
|
You experience installation problems and would like to consult the error log. |
The error messages are located in the following folder: C:\Users\<username>\AppData\Local Look for the file called: \Metasys_System_Configuration_Tool_<xxxxxxxxxxxxx>.html. |
|
|
You receive the following error message when installing SCT: Metasys System Configuration Tool (SCT) previous version detected. Please remove SCT and then run this setup again. |
A previous version of SCT is installed on the computer. You must uninstall any previous version of SCT before installing. Follow the directions in the Uninstalling existing SCT release 11.0 or earlier software and Uninstalling existing NAE/NIE update tool software sections and try the installation again. |
|
|
You receive the following error message when installing SCT: No valid MSSQL Server instances found on the local machine. |
There are two instances that cause this error to occur:
Cancel the installation and see SQL Server Software to review the supported versions of SQL Server. Then, upgrade to a supported version before you proceed with the SCT installation. |
|
|
Installation of SCT 13.0 and later fails. The SCT error log displays the following error: DISMHelper: [datetime] ERROR – Could not load file or assembly ‘System.Management.Automation, Version=3.0.0. |
For Windows 7 x64 operating systems, the Windows Management Framework (WMF) 5.1 or later is required prior to installing SCT. The WMF 5.1 software package is available at this link: https://www.microsoft.com/en-us/download/details.aspx?id=54616 |
|
|
The SCT installation fails and the SCT install log contains the following error if you click View all: DISMHelper:[2019-03-21T11:12:37] ERROR - 0x800f080c Or the following error appears when you launch SCT from the Launcher: Check network connections. Check proxy settings in options. |
Windows 10 version 1809 uses a new method to install the Simple Network Management Protocol (SNMP) feature, which has components that SCT requires. To use the SCT on Windows 10 version 1809, it is best practice to install SCT Release 13.2. You can install SCT Release 13.0 on Windows 10 version 1809, but you must first complete the steps described in Flash Sheet: System Configuration Tool (SCT) installation fails on Microsoft® Windows® 10 version 1809 (LIT-2019F1) or contact your local Johnson Controls representative. You cannot install SCT Release 12.0 or earlier on Windows 10 version 1809. |
|
|
The SCT installation fails and the SCT install log contains the following error: ExecuteSqlDuringInstall: ERROR - The database could not be exclusively locked to perform the operation. |
Complete the following steps to stop the Action Queue service:
After the Action Queue service stops, try the installation again. |
|
|
In the SQL Server Management Studio, SQL Server Agent has the following text after it: (Agent XPs disabled) |
CTOOLS is a 16-bit program and is not supported on any 64-bit operating system. Click OK to close the user message window. |
|
|
During the installation of Windows 8.1 features, a Windows Features dialog box appears that reads: Windows needs files from Windows Update to finish installing some features. Two choices are given: Download files from Windows Update Don't connect to Windows Update |
This is normal. This text appears if you install SQL Server software without Notification Services, which is not required for the SCT. |
|
|
One of these error messages appear when you try to log in to the Site Management Portal: HTTP 404 File not found Internet Information Services Page cannot be found |
Windows 8.1 is trying unsuccessfully to access the Internet to retrieve .NET Framework version 3.5.1 files or other necessary updates. Select either choice and refer to Installing Required Features without Internet Connection for Windows 8.1 in the Metasys Server Installation and Upgrade Instructions PDF (LIT-12012162) for further instructions. |
|
|
While using the SQL Installer tool, you receive a user or error message during SQL Server software installation or upgrade. Possible messages include: SQL Server Install error Instance Name already installed Install failed - Missing Windows Installer 4.5 Install failed - Missing .NET 3.5.1 SP1 No new features were installed during the setup execution The OS does not meet the minimum requirements for this SQL Server install Install failed - Bad software key WARNING: Please install the following prerequisites: .NET 3.5.1 SP1, Windows Installer 4.5 |
To eliminate either of these errors, follow these steps:
|
|
|
While using the SQL Installer tool, you experience installation problems after you edit the text in the Command Line Options window of the SQL Installer. |
Consult the error log file. The error messages file is located in the following folder: C:\Program Files\Microsoft SQL Server\<number based on the SQL release>\Setup Bootstrap\Log\Summary.txt Correct the problem and try the SQL Server installation or upgrade again. |
|
|
You receive the following error message while installing SCT: Metasys NAE/NIE Update Tool (NUT) previous version detected. Please remove NUT and then run this setup again. |
The text within the Command Line Options window contains errors. Correct the errors or restart the SQL Installer so that the Command Line Options window defaults to its original content. |
|
|
The SCT software does not function correctly after you do one of the following:
|
A previous version of the NAE/NIE Update Tool is installed on the computer. You must uninstall prior versions of the NAE/NIE Update Tool before installing SCT. Follow the directions in the Uninstalling existing NAE/NIE update tool software section and try the installation again. |
|
|
After you upgrade to a newer version of SQL Server, SCT no longer starts. |
To correctly change your SQL Server software outside the usual installation or upgrade process, follow these steps:
If you have already changed SQL Server software without uninstalling the SCT, follow these steps:
|
|
|
The following error appears when you try to log in to the SCT: Unable to Authorize Active Directory User. |
To correctly change your SQL Server software outside the usual installation or upgrade process, follow these steps:
If you have already changed SQL Server software without uninstalling the SCT, follow these steps:
|
|
|
The following error appears when you try to log in to the SCT: Error: Unable to Login. Unexpected Error. |
The user may have recently changed the password of their Active
Directory® (AD) domain account, their account is locked out, or their account does not have sufficient privileges. To work around this problem, follow these steps:
Solution 1: The Internet Explorer web browser proxy setting is set to bypass the proxy server for local addresses. To resolve this problem, start the browser and select Tools > Internet Options. Click the Connections tab, then LAN Settings. On the Local Area Network Settings window, select Automatically Detect Settings and select Use automatic configuration script. Type the address of the proxy server. Then, clear both check boxes under the Proxy server section. Relaunch the browser. Solution 2: The URL of the SCT you entered included a space. Remove the space and reload the page. Solution 3: The Launcher is configured to use a proxy server, even though the network does not require a proxy server. Open the Launcher and click the Network Settings button. On the Network Settings window, select Use browser settings. Solution 4: Microsoft SQL Server is not running. Start the SQL Server service with the SQL Server Configuration Manager. |
|
|
(Continued) The following error appears when you try to log in to the SCT: Error: Unable to Login. Unexpected Error. |
Solution 5: SQL Server is missing from the computer’s Path variable. To resolve this problem, follow these steps:
For SQL Server software, the path is as follows: ;C:\Program Files\Microsoft SQL Server\MSSQL10_50.MSSQLSERVER\MSSQL\Binn. For SQL Server 2012 software, the path is as follows: ;C:\Program Files\Microsoft SQL Server\MSSQL11.MSSQLSERVER\MSSQL\Binn. Solution 6: The computer contains files from an earlier operating system or from an earlier version of Metasys software that are conflicting with the updated software. Verify that a folder with an older OS does not exist on the hard disk (for example, WINDOWS.OLD). |
|
|
You change the default language of the SCT, but when you log in, you do not see the new default language. |
Solution 1: SCT has become corrupted and access to the Metasys system folder is broken. To resolve this problem, uninstall SCT then reinstall it. Solution 2: The computer is using an older version of the Internet Explorer web browser. Upgrade the browser to version 11. |
|
|
The following error appears when you launch SCT from the Launcher: Missing Resource File. |
To resolve this problem:
|
|
|
The following error appears when you launch SCT from the Launcher: HTTP Error 500.19 - Internal Server Error The requested page cannot be accessed because the related configuration data for the page is invalid. |
You are trying to use an older version of Launcher that is not compatible with this SCT release. Uninstall the old version of Launcher, then try again. Or to have the latest Launcher pushed to your computer directly from the SCT computer, open the browser and go to http://<sct computer name or IP address>/launcher.msi. |
|
| The Software Manager Notice dialog box appears when you launch SCT. |
To resolve this problem:
|
|