Summary of changes - Metasys - LIT-12012067 - Configuration software - SCT System Configuration Tool - 13.2

SCT Installation and Upgrade Instructions

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12012067
Version
13.2
Revision date
2019-10-14

The following information is new or revised:

  • Added additional steps that you must perform to install the SCT on Windows 10 version 1809. See Operating system requirements.
  • Added note to state that for Windows 7 x64 operating systems, the Windows Management Framework (WMF) 5.1 or later is required prior to installing SCT.
  • Added support for SQL Server 2017 Standard and Express.
  • Added product warranty and patent information to the end of the document.