Getting started - Metasys - LIT-12012067 - Configuration software - SCT System Configuration Tool - 13.2

SCT Installation and Upgrade Instructions

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
Installation Guide
Document number
LIT-12012067
Version
13.2
Revision date
2019-10-14

The Metasys System Configuration Tool Setup is a comprehensive utility that includes several of the Microsoft Windows® components are required for the SCT. The following table outlines the components and products that the Metasys System Configuration Tool Setup installs.

Table 1. Components installed by the Metasys System Configuration Tool setup

Windows Components Installed

Metasys Products Installed

Microsoft Internet Information Services (IIS)

Microsoft .NET Framework 4.6.1

Microsoft Visual C++ Runtime Libraries

Microsoft Message Queuing (MSMQ)

Microsoft SQL Server® 2014 Express with SP3 (64-bit) - Desktop Operating Systems only. Only installs if no version of SQL Server is detected.

System Configuration Tool 13.2

SCT Pro 10.2

Metasys User Interface (UI) Offline 4.1

Launcher 1.7

Software Manager 2.1

NAE/NIE Update Tool 13.2

Metasys Engine Importer

Package Importer