Verifying Your Computer Has a Supported Version of SQL Server Software Installed - Metasys - LIT-12012067 - Configuration software - SCT System Configuration Tool - 13.2

SCT Installation and Upgrade Instructions

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
Installation Guide
Document number
LIT-12012067
Version
13.2
Revision date
2019-10-14

When using the OAS on a virtual machine, if you are installing OAS on a Windows desktop OS, SQL Server 2014 Express SP3 is installed automatically. However, if you are installing OAS on a Windows Server OS, you need to have a supported version of SQL Server software installed. To verify your computer has a supported version of SQL Server Software installed, perform the following steps:

  1. Open the SQL Server Configuration Manager tool.
    Note: If you do not see any version of Microsoft SQL Server on your computer, you do not have this required software. Follow the instructions in this document for installing a supported version of SQL Server software.
  2. In the left pane, select SQL Server Services. In the right pane, double-click the SQL Server instance name.
  3. Click the Advanced tab and scroll down to the Version row.
  4. If the version matches any of the listed version numbers, you have a supported version of SQL Server software. Verify that the version number is any one of the following:
    • 14.0.3238.1 (SQL Server 2017)
    • 13.0.5026.0 (SQL Server 2016 SP2)
    • 12.0.6024.0 (SQL Server 2014 SP3)
    • 11.x.7001.x (SQL Server 2012 SP4)

    If the version does not match any of these version numbers, you need to either apply the required service pack or upgrade to a newer version of SQL Server software. Follow the instructions in this document for installing a supported version of SQL Server software.