Security certificate warnings - Metasys - LIT-12012067 - Configuration software - SCT System Configuration Tool - 13.2

SCT Installation and Upgrade Instructions

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12012067
Version
13.2
Revision date
2019-10-14
Note: Ensure that your web browser has cookies enabled before browsing to the Metasys UI Offline or the SCT Pro.

When browsing to the Metasys UI Offline or the SCT Pro, your web browser displays a security certificate warning if your Metasys UI Offline and SCT Pro site does not have a trusted security certificate. If you enter localhost as the server name, your web browser displays a security certificate warning even if you install a trusted security certificate.

If you see this warning, browse to the Metasys UI Offline or the SCT Pro site by doing the following:
  • For Google® Chrome™ browser:
    1. Tap or click Advanced.
    2. Tap or click Proceed to [name or IP Address], where [name or IP Address] is the computer name or IP address of the computer on which the SCT is installed. The Metasys UI Offline or the SCT Pro login screen appears.
  • For Windows Internet Explorer 11 or Microsoft Edge, tap or click Continue to this website (not recommended). The Metasys UI or the SCT Pro login screen appears.
  • For Apple® Safari® browser: tap or click Continue in the Cannot Verify Server Identity window. The Metasys UI Offline or the SCT Pro login screen appears.
Note: The Metasys UI Offline does not support autofill functionality for the username or password fields.

For more information about implementing security certificates for the Metasys UI or the SCT Pro sites, refer to the Appendix: Security Certificate Implementation section of the Network and IT Guidance Technical Bulletin (LIT-12011279) .