Dynamically Creatable: No
Dynamically Deletable: No
|
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
|---|---|---|---|---|---|---|---|
| CHANGES_PENDING | X | 416 | Boolean | ||||
| LINK_SPEED | X | 420 | Real | ||||
| NETWORK_TYPE | X | 427 | Enumerated | ||||
| OUT_OF_SERVICE | X | 81 | Boolean | ||||
| PROTOCOL_LEVEL | X | 482 | Enumerated | ||||
| RELIABILITY | X | 103 | Enumerated | ||||
| STATUS_FLAGS | X | 111 | BitString | ||||
| APDU_LENGTH | X | 399 | Unsigned | ||||
| BACNET_COMMAND | X | 417 | Enumerated | X | |||
| BACNET_IP_ADDRESS | X | 400 | Octet String | ||||
| BACNET_MAC_ADDRESS | X | 423 | Octet String | ||||
| IP_DEFAULT_GATEWAY | X | 401 | Octet String | ||||
| IP_DNS_SERVER | X | 406 | Octet String | ||||
| IP_SUBNET_MASK | X | 411 | Octet String | ||||
| NETWORK_NUMBER | X | 425 | Unsigned16 | X | |||
| NETWORK_NUMBER_QUALITY | X | 426 | Enumerated | ||||
| ADVANCED_LOGGING_ENABLED | X | 1894 | Boolean | X | |||
| BROADCAST_RECEIVES | X | 2047 | Unsigned | ||||
| BROADCAST_TRANSMITS | X | 2046 | Unsigned | ||||
| BROADCASTS_FORWARDED_BY_HUB_FUNCTION | X | 1893 | Unsigned | ||||
| CONFIGURATION_STATUS | X | 1990 | Enumerated | X | |||
| COV_COUNT | X | 839 | Unsigned | ||||
| COV_THRESHOLD | X | 1161 | Unsigned | X | |||
| DATA_RECORD_DELETE | X | 3058 | Boolean | ||||
| DATALINK_TYPE | X | 1168 | Unsigned | ||||
| DEBUG_MODE | X | 2033 | Boolean | X | |||
| DEBUG_TIME_REMAINING | X | 1750 | Unsigned | ||||
| RCV_MSG_DISCARD | X | 3850 | Unsigned | ||||
| ENABLE_DATALINK_RECOVERY_LOGIC | X | 1898 | Boolean | X | |||
| ETHERNET_PORT_IN_USE | X | 1909 |
Enumerated |
||||
| INTERNODE_COMM_TIMER | X | 825 | Byte | X | |||
| JCI_MAX_BVLC_LENGTH_ACCEPTED_ | X | 1855 | Unsigned | ||||
| JCI_MAX_NPDU_LENGTH_ACCEPTED | X | 1858 | Unsigned | ||||
| JCI_NETWORK_PORT_APDU_RETRIES | X | 1851 | Byte | X | |||
| JCI_NETWORK_PORT_APDU_SEGMENT_TIMEOUT | X | 1849 | Unsigned | X | |||
| JCI_NETWORK_PORT_APDU_TIMEOUT | X | 1849 | Unsigned | X | |||
| JCI_NPO_ATTRIBUTES_REQUIRING_ACTIVATION | X | 2000 | List | ||||
| JCI_NPO_CHANGES_PENDING_BITSTRING | X | 1852 | Byte | ||||
| JCI_SECURE_CONNECT_ACCEPTING_HEARTBEAT_TIMEOUT | X | 1875 | Unsigned | X | 3-500 seconds | ||
| JCI_SECURE_CONNECT_CONNECT_WAIT_TIMEOUT | X | 1872 | Unsigned | X | 5-300 seconds | ||
| JCI_SECURE_CONNECT_DIRECT_CONNECT_ACCEPT_URIS | X | 1864 | Character String | ||||
| JCI_SECURE_CONNECT_DIRECT_CONNECT_CONNECTION_STATUS | X | 1866 | List | ||||
| JCI_SECURE_CONNECT_DIRECT_CONNECT_ENABLE | X | 1871 | Boolean | X | |||
| JCI_SECURE_CONNECT_DISCONNECT_WAIT_TIMEOUT | X | 1873 | Unsigned | X | 5-300 seconds | ||
| JCI_SECURE_CONNECT_FAILOVER_HUB_STATUS | X | 1861 | Structure | ||||
| JCI_SECURE_CONNECT_FAILOVER_HUB_URI | X | 1859 | Character String | X | |||
| JCI_SECURE_CONNECT_HUB_CONNECTOR_STATE | X | 1857 | Enumerated | ||||
| JCI_SECURE_CONNECT_HUB_FUNCTION_ACCEPT_URIS | X | 1863 | Character String | ||||
| JCI_SECURE_CONNECT_HUB_FUNCTION_CONNECTION_STATUS | X | 1865 | List | ||||
| JCI_SECURE_CONNECT_HUB_FUNCTION_ENABLE | X | 1862 | Boolean | X | |||
| JCI_SECURE_CONNECT_INITIATING_HEARTBEAT_TIMEOUT | X | 1874 | Unsigned | X | 3-300 seconds | ||
| JCI_SECURE_CONNECT_MAXIMUM_RECONNECT_TIME | X | 1878 | Unsigned | X | 2-300 seconds | ||
| JCI_SECURE_CONNECT_MINIMUM_RECONNECT_TIME | X | 1877 | Unsigned | X | 2-300 seconds | ||
| JCI_SECURE_CONNECT_NODE_TYPE | X | 1867 | Enumerated | ||||
| JCI_SECURE_CONNECT_PRIMARY_HUB_STATUS | X | 1860 | Structure | ||||
| JCI_SECURE_CONNECT_PRIMARY_HUB_URI | X | 1856 | Character String | X | |||
| MASTER | X | 1059 | Boolean | ||||
| MAXIMUM_DIRECT_CONNECTION_RETRIES | X | 1889 | Unsigned | X | |||
| MESSAGE_RECEIVES | X | 1143 | Unsigned | ||||
| MESSAGE_TRANSMITS | X | 1142 | Unsigned | ||||
| MESSAGES_FORWARDED_BY_HUB_FUNCTION | X | 1892 | Unsigned | ||||
| NETWORK_ADDRESS | X | 875 | Unsigned | ||||
| NETWORK_PORT_WEBSOCKET_URIS | X | 1879 | List | ||||
| NUMBER_OF_ACTIVE_WEBSOCKET_CONNECTIONS | X | 1891 | Unsigned | ||||
| NUMBER_OF_DATALINK_RECOVERY_EVENTS | X | 1897 | Enumerated | ||||
| NUMBER_OF_PENDING_DIRECT_CONNECTIONS | X | 1890 | Unsigned | ||||
| PEAK_COV_CACHE_COUNT | X | 856 | Unsigned | ||||
| PEAK_COV_COUNT | X | 851 | Unsigned | ||||
| RESET_DATE | X | 1141 | Date | ||||
| RESET_TIME | X | 1140 | Time | ||||
| SECURE_CONNECT_HUB_RECONNECT_TIMER_STATUS | X | 1896 | Enumerated | ||||
| SECURE_CONNECT_PENDING_NODE_TYPE | X | 1870 | Enumerated | ||||
| SECURE_PORT_NUM | X | 1869 | Unsigned | X | 1-65535 | ||
| TRANSMIT_FAILURES | X | 2048 | Unsigned | ||||
| UNSECURE_NPDUS_RECEIVED | X | 1999 | Unsigned | ||||
| USE_SITE_SETTINGS | X | 1995 | Boolean | X | |||
| VIRTUAL_MAC_ADDRESS | X | 1868 | Octet String | ||||
| WEBSOCKET_SERVER_TASK_STATE | X | 1880 | List |