Dynamically Creatable: No
Dynamically Deletable: No
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
---|---|---|---|---|---|---|---|
NUMBER_OF_STATES |
X |
74 |
X |
2–500 1 |
|||
OBJECT_NAME |
X |
77 |
X |
||||
OUT_OF_SERVICE |
X |
81 |
X |
||||
PRESENT_VALUE |
X |
85 |
X 2 |
||||
ACKED_TRANSITIONS 3 |
X |
0 |
|||||
ALARM_VALUES3 |
X |
7 |
X 4 |
0–65,535 |
|||
DESCRIPTION |
X |
28 |
X |
64 characters max |
|||
DEVICE_TYPE |
X |
31 |
X |
20 characters max |
|||
EVENT_DETECTION_ENABLE3 | X | 353 | |||||
EVENT_ENABLE3 |
X |
35 |
X4 |
||||
EVENT_MESSAGE_TEXTS3 |
X |
351 |
|||||
EVENT_MESSAGE_TEXTS_ CONFIG3 |
X |
352 |
X4 | 256 characters max | |||
EVENT_TIME_STAMPS3 |
X |
130 |
|||||
FAULT_VALUES3 |
X |
39 |
X4 |
0–65,535 |
|||
NOTIFICATION_CLASS3 |
X |
17 |
X4 |
1–4,194,303 |
|||
NOTIFY_TYPE3 |
X |
72 |
X4 |
||||
PROFILE_NAME |
X |
168 |
|||||
RELIABILITY |
X |
103 |
X2 |
||||
STATE_TEXT |
X |
110 |
|||||
TIME_DELAY3 |
X |
113 |
X4 |
0–65,535 |
|||
ALARM_MESSAGE_TEXT |
X |
536 |
Character String |
X4 |
|||
ALARM_STATE |
X |
1006 |
Enumerated |
||||
ENABLED |
X |
673 |
Boolean |
X |
|||
EXECUTION_PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
GRAPHIC |
X |
32581 |
Object Reference |
X4 |
|||
GRAPHIC_ALIAS |
X |
32623 |
Character String |
X4 |
|||
INSTANCE_NUMBER |
X |
32589 |
Unsigned |
X |
|||
INTERFACE_VALUE |
X |
4265 |
Enumerated |
||||
INTRINSIC_ALARM_DISABLED |
X |
4305 |
Boolean |
X |
|||
ITEM_REFERENCE |
X |
32527 |
Character String |
||||
LAST_KNOWN_TIME_STAMPS |
X |
1290 |
BACnet Array |
||||
MAPPED_NAME 5 |
X |
2564 |
String |
||||
NET_N2_ADDRESS |
X |
806 |
Byte |
||||
NET_POINT_ADDR |
X |
808 |
Unsigned |
||||
NET_POINT_TYPE |
X |
807 |
Enumerated |
||||
NOTIFICATION_OBJ_REF |
X |
4304 |
Object Reference |
X |
|||
OBJECT_CATEGORY |
X |
908 |
Enumerated |
X |
|||
OFFLINE |
X |
913 |
Boolean |
||||
OUT_OF_SERVICE_EXPIRATION_TIME |
X |
64787 |
Complex |
||||
OVERRIDDEN |
X |
809 |
Boolean |
||||
OVERRIDE_EXPIRATION_TIME |
X |
64786 |
Complex |
||||
REMOTE_DESCRIPTION |
X |
32519 |
Character String |
X |
|||
REMOTE_DEVICE_ADDRESS5 |
X |
538 |
Complex |
||||
STATES_TEXT |
X |
931 |
Enumerated |
X |
|||
STATES_TEXT_ERROR_STATUS |
X |
64022 |
Enumerated |
||||
STATUS |
X |
512 |
Enumerated |
||||
STORED_EVENT_ENABLE |
X |
4306 |
BitString |
||||
TRUNK_NUMBER |
X |
549 |
Unsigned |
||||
USER_NAME |
X |
2390 |
Character String |
X |
|||
USER_SELECTED_STATES_TEXT |
X |
1103 |
Boolean |
X |