Dynamically Creatable: No
Dynamically Deletable: No
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
---|---|---|---|---|---|---|---|
OBJECT_NAME |
X |
77 |
X |
||||
PRESENT_VALUE |
X |
85 |
X |
||||
UNITS |
X |
117 |
X |
0–65,535 |
|||
ACKED_TRANSITIONS 1 |
X |
0 |
|||||
COV_INCREMENT |
X |
22 |
X |
any value > 0 |
|||
CURRENT_COMMAND_PRIORITY |
X |
431 |
|||||
DEADBAND |
X |
25 |
X 2 |
||||
DESCRIPTION |
X |
28 |
X |
64 characters max |
|||
EVENT_DETECTION_ENABLE1 | X | 353 | |||||
EVENT_ENABLE1 |
X |
35 |
X2 |
||||
EVENT_MESSAGE_TEXTS1 |
X |
351 | |||||
EVENT_MESSAGE_TEXTS_ CONFIG1 | X | 352 | X2 | 256 characters max | |||
EVENT_STATE1 |
X |
36 |
|||||
EVENT_TIME_STAMPS1 |
X |
130 |
|||||
HIGH_LIMIT1 |
X |
45 |
X2 |
||||
LIMIT_ENABLE1 |
X |
52 |
X2 |
||||
LOW_LIMIT1 |
X |
59 |
X2 |
||||
MAX_PRES_VALUE |
X |
65 |
X |
||||
MIN_PRES_VALUE |
X |
69 |
X |
||||
NOTIFICATION_CLASS1 |
X |
17 |
X2 |
1–4,194,303 |
|||
NOTIFY_TYPE1 |
X |
72 |
X2 |
||||
OUT_OF_SERVICE |
X |
81 |
X |
||||
PRIORITY_ARRAY |
X |
87 | |||||
PROFILE_NAME |
X |
168 |
|||||
RELIABILITY |
X |
103 |
X |
||||
RELINQUISH_DEFAULT |
X |
104 |
X |
||||
TIME_DELAY1 |
X |
113 |
X2 |
0–65,535 |
|||
ALARM_MESSAGE_TEXT |
X |
536 |
Character String |
X2 |
|||
ALARM_STATE |
X |
1006 |
Enumerated |
||||
ENABLED |
X |
673 |
Boolean |
X |
|||
EXECUTION_PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
GRAPHIC |
X |
32581 |
Object Reference |
X2 |
|||
GRAPHIC_ALIAS |
X |
32623 |
Character String |
X2 |
|||
INSTANCE_NUMBER |
X |
32589 |
Unsigned |
||||
INTRINSIC_ALARM_DISABLED |
X |
4305 |
Boolean |
X |
|||
ITEM_REFERENCE |
X |
32527 |
Character String |
||||
LAST_KNOWN_TIME_STAMPS |
X |
1290 |
BACnet Array |
||||
MAPPED_NAME 3 |
X |
2564 |
String |
||||
NOTIFICATION_OBJ |
X |
4304 |
Object Reference |
||||
OBJECT_CATEGORY |
X |
908 |
Enumerated |
||||
OUT_OF_SERVICE_EXPIRATION_TIME |
X |
64787 |
Complex |
||||
OVERRIDE_EXPIRATION_TIME |
X |
64786 |
Complex |
||||
REMOTE_DESCRIPTION3 |
X |
32519 |
Character String |
X |
|||
REMOTE_DEVICE_ADDRESS3 |
X |
538 |
String |
||||
STATUS |
X |
512 |
Enumerated |
||||
STORED_EVENT_ENABLE |
X |
4306 |
BitString |
||||
USER_NAME |
X |
2390 |
Character String |
X |
400 characters max |