Dynamically Creatable: No
Dynamically Deletable: No
|
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
|---|---|---|---|---|---|---|---|
|
OBJECT_NAME |
X |
77 |
X |
||||
|
OUT_OF_SERVICE |
X |
81 |
X |
||||
|
POLARITY |
X |
84 |
X |
||||
|
PRESENT_VALUE |
X |
85 |
X |
||||
|
RELINQUISH_DEFAULT |
X |
104 |
X |
||||
|
ACKED_TRANSITIONS 1 |
X |
0 |
|||||
|
ACTIVE_TEXT |
X |
4 |
|||||
|
ACTIVE_TIME_RESET |
X |
114 |
X |
||||
|
COS_COUNT |
X |
15 |
X |
||||
|
COS_TIME |
X |
16 | |||||
|
DESCRIPTION |
X |
28 |
X |
64 characters max |
|||
|
DEVICE_TYPE |
X |
31 |
X |
20 characters max |
|||
|
ELAPSED_ACTIVE_TIME |
X |
33 |
X |
||||
| EVENT_DETECTION_ENABLE | X | 353 | |||||
|
EVENT_ENABLE1 |
X |
35 |
X 2 |
||||
|
EVENT_MESSAGE_TEXTS1 |
X |
351 | |||||
| EVENT_MESSAGE_TEXTS_ CONFIG | X | 352 | X2 | 256 characters max | |||
|
EVENT_TIME_STAMPS1 |
X |
130 |
|||||
|
FEEDBACK_VALUE1 |
X |
40 |
X2 |
||||
|
INACTIVE_TEXT |
X |
46 |
|||||
|
MIN_OFF_TIME |
X |
66 |
X |
||||
|
MIN_ON_TIME |
X |
67 |
X |
||||
|
NOTIFICATION_CLASS1 |
X |
17 |
X2 |
1–4,194,303 |
|||
|
NOTIFY_TYPE1 |
X |
72 |
X2 |
||||
|
RELIABILITY |
X |
103 |
X |
||||
|
STATE_COUNT_RESET |
X |
115 |
X |
||||
|
TIME_DELAY1 |
X |
113 |
X2 |
0–65,535 |
|||
|
ALARM_MESSAGE_TEXT1 |
X |
536 |
Character String |
X2 |
|||
|
ALARM_STATE |
X |
1006 |
Enumerated |
||||
|
BACNET_EXPOSED |
X |
3807 |
Boolean |
X |
|||
|
ENABLED |
X |
673 |
Boolean |
X |
|||
|
ERROR_STATUS |
X |
576 |
Enumerated |
||||
|
EXECUTION_PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
|
FEEDBACK_REFERENCE |
X |
753 |
Attribute Reference |
||||
|
GRAPHIC |
X |
32581 |
Object Reference |
X2 |
|||
|
GRAPHIC_ALIAS |
X |
32623 |
Character String |
X2 |
|||
|
HEAVY_EQUIP_DELAY |
X |
516 |
Unsigned |
X |
|||
|
HED_CONTROLLER |
X |
517 |
Unsigned |
X |
|||
|
IGNORE_RELINQUISH_ DEFAULT |
X |
580 |
Boolean |
X |
|||
|
ITEM_REFERENCE |
X |
32527 |
Character String |
||||
|
INTRINSIC_ALARM_DISABLED |
X |
4305 |
Boolean |
X |
|||
|
MINIMUM_CYCLE_TIME |
X |
2199 |
Unsigned |
X |
|||
|
NOTIFICATION_OBJ_REF |
X |
4304 |
Object Reference |
X |
|||
|
OBJECT_CATEGORY |
X |
908 |
Enumerated |
X |
|||
|
OFFLINE |
X |
913 |
Boolean |
||||
|
OUTPUT |
X |
663 |
Boolean |
||||
|
OVERRIDE_EXPIRATION_TIME |
X |
64786 |
Structure |
||||
|
PULSE_WIDTH |
X |
600 |
Real |
X |
|||
|
RESTORE_COMMAND_ PRIORITY |
X |
721 |
Bit String |
X |
|||
|
SAB_MAC_ADDR |
X |
3645 |
Unsigned |
||||
|
SETUP |
X |
518 |
Enumerated |
||||
|
SLOT_A |
X |
990 |
Unsigned |
||||
|
SLOT_B |
X |
991 |
Unsigned |
||||
|
STARTUP_OFF_STATE_ENABLE |
X |
1229 |
Boolean |
X |
|||
|
STATES_TEXT |
X |
931 |
Enumerated |
X 3 |
|||
|
STATUS |
X |
512 |
Enumerated |
||||
|
STORED_EVENT_ENABLE |
X |
4306 |
Bit String |
||||
|
USER_NAME |
X |
2390 |
Character String |
X |
400 characters max |