Dynamically Creatable: No
Dynamically Deletable: No
|
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
|---|---|---|---|---|---|---|---|
|
OBJECT_NAME |
X |
77 |
X |
||||
|
OUT_OF_SERVICE |
X |
81 |
X 1 |
||||
|
PRESENT_VALUE |
X |
85 |
X1 |
||||
|
UNITS |
X |
117 |
X |
0–65,535 |
|||
|
ACKED_TRANSITIONS 2 |
X |
0 |
|||||
|
COV_INCREMENT |
X |
22 |
X |
any value > 0 |
|||
|
CURRENT_COMMAND_PRIORITY |
X |
431 |
|||||
|
DEADBAND2 |
X |
25 |
X 3 |
||||
|
DESCRIPTION |
X |
28 |
X |
64 characters max |
|||
| EVENT_DETECTION_ENABLE2 | X |
353 |
|||||
|
EVENT_ENABLE2 |
X |
35 |
X1 |
||||
|
EVENT_MESSAGE_TEXTS2 |
X |
351 |
|||||
| EVENT_MESSAGE_TEXTS_ CONFIG2 |
X |
352 |
X1 |
256 characters |
|||
|
EVENT_TIME_STAMPS2 |
X |
130 |
|||||
|
HIGH_LIMIT2 |
X |
45 |
X1 |
||||
|
LIMIT_ENABLE2 |
X |
52 |
X1 |
||||
|
LOW_LIMIT2 |
X |
59 |
X1 |
||||
|
MAX_PRES_VALUE |
X |
65 |
Float |
X |
|||
|
MIN_PRES_VALUE |
X |
69 |
Float |
X |
|||
|
NOTIFICATION_CLASS2 |
X |
17 |
X1 |
1–4,194,303 |
|||
|
NOTIFY_TYPE2 |
X |
72 |
X1 |
||||
|
PRIORITY_ARRAY 4 |
X |
87 |
|||||
|
RELIABILITY |
X |
103 |
X1 |
||||
|
RELINQUISH_DEFAULT4 |
X |
104 |
X |
||||
|
TIME_DELAY |
X |
113 |
X |
0–65,535 |
|||
|
ALARM_MESSAGE_TEXT |
X |
536 |
Character String |
X1 |
|||
|
ALARM_STATE |
X |
1006 |
Enumerated |
||||
|
BACNET_EXPOSED |
X |
3807 |
Boolean |
X |
|||
|
CONNECTED_STATUS |
X |
1243 |
Enumerated |
||||
|
CONNECTED_TO |
X |
1376 |
Attribute Reference |
X1 |
|||
|
CONNECTED_TO_INTERNAL_ APPLICATION |
X |
6081 |
Enumerated |
||||
|
DEFAULT_VALUE |
X |
3113 |
Real |
X |
|||
|
DIRECTION |
X |
746 |
Enumerated |
X1 |
|||
|
DISPLAY_PRECISION |
X |
661 |
Enumerated |
X |
0–12 |
||
|
ENABLED |
X |
673 |
Boolean |
X |
|||
|
EXECUTION_PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
|
FAILSOFT4 |
X |
2567 |
Boolean |
||||
|
FAILSOFT_CURRENTLY_ACTIVE4 |
X |
6088 |
Enumerated |
||||
|
GRAPHIC |
X |
32581 |
Object Reference |
X1 |
|||
|
GRAPHIC_ALIAS |
X |
32623 |
Character String |
X1 |
|||
|
INSTANCE_NUMBER4 |
X |
32589 |
Unsigned |
||||
|
INTRINSIC_ALARM_DISABLED4 |
X |
4305 |
Boolean |
X |
|||
|
ITEM_REFERENCE |
X |
32527 |
Character String |
||||
|
NOTIFICATION_OBJ_REF |
X |
4304 |
Object Reference |
X |
|||
|
OBJECT_CATEGORY |
X |
908 |
Enumerated |
X |
|||
|
OUT_OF_SERVICE_EXPIRATION_TIME4 |
X |
64787 |
Structure |
||||
|
OVERRIDE_EXPIRATION_TIME4 |
X |
64786 |
Structure |
||||
|
PRESENT_VALUE_WRITABLE |
X |
6080 |
Structure |
||||
|
PRIORITY_FOR_WRITING_TO_ CONNECTED |
X |
6093 |
Byte |
X1 |
|||
|
PRIORITY_SUPPORTED |
X |
6083 |
Boolean |
X1 |
|||
|
PROPERTY_REF_VALUE |
X |
2202 |
Attribute Reference |
||||
|
REFERENCED_RELIABILITY4 |
X |
6085 |
Enumerated |
||||
|
REFERENCED_VALUE4 |
X |
6084 |
Real |
||||
|
REFERENCED_VALUE_COS_ COUNT4 |
X |
6086 |
Unsigned |
||||
|
RESTORE_COMMAND_ PRIORITY4 |
X |
721 |
Bit String |
X |
|||
|
STATUS |
X |
512 |
Enumerated |
||||
|
STORED_EVENT_ENABLE |
X |
4306 |
Bit String |
||||
|
USE_COV_MIN_SEND_TIME4 |
X |
3930 |
Boolean |
X |
|||
|
USER_NAME |
X |
2390 |
Character String |
X |
400 characters max |