Character Sets Supported - Metasys - LIT-12013310 - Server - Open Application Server - 13.0

Open Application Server (OAS) Protocol Implementation Conformance Statement

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013310
Version
13.0
Revision date
2023-11-08
Product status
Active

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

ISO 10646 (UTF-8)

IBM®/ Microsoft® Double-Byte Character Set (DBCS)

ISO 8859-1

ISO 10646 Universal Character Set-2 (UCS-2)

ISO 10646 (UCS-4)

Japanese Industrial Standard (JIS) X 0208