BACnet Secure Connect - Annex AB - Metasys - LIT-12013310 - Server - Open Application Server - 13.0

Open Application Server (OAS) Protocol Implementation Conformance Statement

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013310
Version
13.0
Revision date
2023-11-08
Product status
Active

BACnet Secure Connect Node

If direct connections are supported:

OAS without integrations

Maximum number of simultaneous direct connections initiated: 200

Maximum number of simultaneous direct connections accepted: 200

OAS with integrations

Maximum number of simultaneous direct connections initiated: 150

Maximum number of simultaneous direct connections accepted: 150

BACnet Secure Connect Hub Function

OAS without integrations

Maximum number of simultaneous hub connections accepted: 200

OAS with integrations

Maximum number of simultaneous hub connections accepted: 150

Additional cipher suites supported beyond those required for TLS V1.3

The additional cipher suites supported using the cipher suite names as of the TLS Cipher Suite Registry at IANA (See RFC 8446):

____________________________________________________________________

Additional Transport Layer Security versions other than V1.3 supported

The TLS versions other than V1.3 that are supported, including the supported cipher suites for the version beyond those required, using the cipher suite names as defined by the TLS version supported:

________________________________________________________________________

Generates private keys internally, and provides matching certificate signing requests.

DNS host name resolution supported (RFC 1123)