Network Port (Secure Connect DataLink) - Metasys - LIT-12013310 - Server - Open Application Server - 12.0

Open Application Server (OAS) Protocol Implementation Conformance Statement

Brand
Metasys
Product name
Open Application Server
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013310
Version
12.0
Revision date
2022-07-06
Product status
Active
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Network Port (Secure Connect Datalink)

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

CHANGES_PENDING X     416 Boolean    
LINK_SPEED X     420 Real    
NETWORK_TYPE X     427 Enumerated    
OUT_OF_SERVICE X     81 Boolean    
PROTOCOL_LEVEL X     482 Enumerated    
RELIABILITY X     103 Enumerated    
STATUS_FLAGS X     111 BitString    
APDU_LENGTH   X   399 Unsigned    
BACNET_COMMAND   X   417 Enumerated X  
BACNET_IP_ADDRESS   X   400 Octet String    
BACNET_MAC_ADDRESS   X   423 Octet String    
IP_DEFAULT_GATEWAY   X   401 Octet String    
IP_DNS_SERVER   X   406 Octet String    
IP_SUBNET_MASK   X   411 Octet String    
NETWORK_NUMBER   X   425 Unsigned16 X  
NETWORK_NUMBER_QUALITY   X   426 Enumerated    
ADVANCED_LOGGING_ENABLED     X 1894 Boolean X  
BROADCAST_RECEIVES     X 2047 Unsigned    
BROADCAST_TRANSMITS     X 2046 Unsigned    
BROADCASTS_FORWARDED_BY_HUB_FUNCTION     X 1893 Unsigned    
CONFIGURATION_STATUS     X 1990 Enumerated X  
COV_COUNT     X 839 Unsigned    
COV_THRESHOLD     X 1161 Unsigned X  
DATA_RECORD_DELETE     X 3058 Boolean    
DATALINK_TYPE     X 1168 Unsigned    
DEBUG_MODE     X 2033 Boolean X  
DEBUG_TIME_REMAINING     X 1750 Unsigned    
DISCARDED_FRAMES     X 2051 Unsigned    
ENABLE_DATALINK_RECOVERY_LOGIC     X 1898 Boolean X  
INTERNODE_COMM_TIMER     X 825 Byte X  
JCI_MAX_BVLC_LENGTH_ACCEPTED_     X 1855 Unsigned    
JCI_MAX_NPDU_LENGTH_ACCEPTED     X 1858 Unsigned    
JCI_NETWORK_PORT_APDU_RETRIES     X 1851 Byte X  
JCI_NETWORK_PORT_APDU_SEGMENT_TIMEOUT     X 1849 Unsigned X  
JCI_NETWORK_PORT_APDU_TIMEOUT     X 1849 Unsigned X  
JCI_NPO_ATTRIBUTES_REQUIRING_ACTIVATION     X 2000 List    
JCI_NPO_CHANGES_PENDING_BITSTRING     X 1852 Byte    
JCI_SECURE_CONNECT_ACCEPTING_HEARTBEAT_TIMEOUT     X 1875 Unsigned X 3-500 seconds
JCI_SECURE_CONNECT_CONNECT_WAIT_TIMEOUT     X 1872 Unsigned X 5-300 seconds
JCI_SECURE_CONNECT_DIRECT_CONNECT_ACCEPT_URIS     X 1864 Character String    
JCI_SECURE_CONNECT_DIRECT_CONNECT_CONNECTION_STATUS     X 1866 List    
JCI_SECURE_CONNECT_DIRECT_CONNECT_ENABLE     X 1871 Boolean X  
JCI_SECURE_CONNECT_DISCONNECT_WAIT_TIMEOUT     X 1873 Unsigned X 5-300 seconds
JCI_SECURE_CONNECT_FAILOVER_HUB_STATUS     X 1861 Structure    
JCI_SECURE_CONNECT_FAILOVER_HUB_URI     X 1859 Character String X  
JCI_SECURE_CONNECT_HUB_CONNECTOR_STATE     X 1857 Enumerated    
JCI_SECURE_CONNECT_HUB_FUNCTION_ACCEPT_URIS     X 1863 Character String    
JCI_SECURE_CONNECT_HUB_FUNCTION_CONNECTION_STATUS     X 1865 List    
JCI_SECURE_CONNECT_HUB_FUNCTION_ENABLE     X 1862 Boolean X  
JCI_SECURE_CONNECT_INITIATING_HEARTBEAT_TIMEOUT     X 1874 Unsigned X 3-300 seconds
JCI_SECURE_CONNECT_MAXIMUM_RECONNECT_TIME     X 1878 Unsigned X 2-300 seconds
JCI_SECURE_CONNECT_MINIMUM_RECONNECT_TIME     X 1877 Unsigned X 2-300 seconds
JCI_SECURE_CONNECT_NODE_TYPE     X 1867 Enumerated    
JCI_SECURE_CONNECT_PRIMARY_HUB_STATUS     X 1860 Structure    
JCI_SECURE_CONNECT_PRIMARY_HUB_URI     X 1856 Character String X  
MASTER     X 1059 Boolean    
MAXIMUM_DIRECT_CONNECTION_RETRIES     X 1889 Unsigned X  
MESSAGE_RECEIVES     X 1143 Unsigned    
MESSAGE_TRANSMITS     X 1142 Unsigned    
MESSAGES_FORWARDED_BY_HUB_FUNCTION     X 1892 Unsigned    
NETWORK_ADDRESS     X 875 Unsigned    
NETWORK_PORT_WEBSOCKET_URIS     X 1879 List    
NUMBER_OF_ACTIVE_WEBSOCKET_CONNECTIONS     X 1891 Unsigned    
NUMBER_OF_DATALINK_RECOVERY_EVENTS     X 1897 Enumerated    
NUMBER_OF_PENDING_DIRECT_CONNECTIONS     X 1890 Unsigned    
PEAK_COV_CACHE_COUNT     X 856 Unsigned    
PEAK_COV_COUNT     X 851 Unsigned    
RESET_DATE     X 1141 Date    
RESET_TIME     X 1140 Time    
SECURE_CONNECT_HUB_RECONNECT_TIMER_STATUS     X 1896 Enumerated    
SECURE_CONNECT_PENDING_NODE_TYPE     X 1870 Enumerated    
SECURE_PORT_NUM     X 1869 Unsigned X 1-65535
TRANSMIT_FAILURES     X 2048 Unsigned    
UNSECURE_NPDUS_RECEIVED     X 1999 Unsigned    
USE_SITE_SETTINGS     X 1995 Boolean X  
VIRTUAL_MAC_ADDRESS     X 1868 Octet String    
WEBSOCKET_SERVER_TASK_STATE     X 1880 List