Multistate Input - Metasys - LIT-12013310 - Server - Open Application Server - 12.0

Open Application Server (OAS) Protocol Implementation Conformance Statement

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013310
Version
12.0
Revision date
2022-07-06
Product status
Active

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Multistate Input

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

NUMBER_OF_STATES

X

   

74

 

X

2–500 1

OBJECT_NAME

X

   

77

 

X

 

OUT_OF_SERVICE

X

    81  

X

 

PRESENT_VALUE

X

    85  

X 2

 

ACKED_TRANSITIONS 3

 

X

 

0

     

ALARM_VALUES3

 

X

 

7

 

X 4

0–65,535

DESCRIPTION

 

X

 

28

 

X

64 characters max

DEVICE_TYPE

 

X

 

31

 

X

20 characters max

EVENT_DETECTION_ENABLE3   X   353      

EVENT_ENABLE3

 

X

 

35

 

X4

 

EVENT_MESSAGE_TEXTS3

 

X

 

351

     

EVENT_MESSAGE_TEXTS_ CONFIG3

 

X

 

352

  X4 256 characters max

EVENT_TIME_STAMPS3

 

X

 

130

     

FAULT_VALUES3

 

X

 

39

 

X4

0–65,535

NOTIFICATION_CLASS3

 

X

 

17

 

X4

1–4,194,303

NOTIFY_TYPE3

 

X

 

72

 

X4

 

PROFILE_NAME

 

X

 

168

     

RELIABILITY

 

X

 

103

 

X2

 

STATE_TEXT

 

X

 

110

     

TIME_DELAY3

 

X

 

113

 

X4

0–65,535

ALARM_MESSAGE_TEXT

   

X

536

Character String

X4

 

ALARM_STATE

   

X

1006

Enumerated

   

ENABLED

   

X

673

Boolean

X

 

EXECUTION_PRIORITY

   

X

2197

Enumerated

X

0–3

GRAPHIC

   

X

32581

Character String

X4

 

GRAPHIC_ALIAS

   

X

32623

Character String

X4

 

INSTANCE_NUMBER

   

X

32589

Unsigned

X

 

INTERFACE_VALUE

   

X

4265

Enumerated

   

INTRINSIC_ALARM_DISABLED

   

X

4305

Boolean

X

 

ITEM_REFERENCE

   

X

32527

Character String

   

LAST_KNOWN_TIME_STAMPS

   

X

1290

BACnet Array

   

MAPPED_NAME 5

   

X

2564

String

   

NET_N2_ADDRESS

   

X

806

Byte

   

NET_POINT_ADDR

   

X

808

Unsigned

   

NET_POINT_TYPE

   

X

807

Enumerated

   

NOTIFICATION_OBJ_REF

   

X

4304

Object Reference

X

 

OBJECT_CATEGORY

   

X

908

Enumerated

X

 

OFFLINE

   

X

913

Boolean

   

OUT_OF_SERVICE_EXPIRATION_TIME

   

X

64787

Complex

   

OVERRIDDEN

   

X

809

Boolean

   

OVERRIDE_EXPIRATION_TIME

   

X

64786

Complex

   

REMOTE_DESCRIPTION

   

X

32519

Character String

X

 

REMOTE_DEVICE_ADDRESS5

   

X

538

Complex

   

STATES_TEXT

   

X

931

Enumerated

X

 

STATES_TEXT_ERROR_STATUS

   

X

64022

Enumerated

   

STATUS

   

X

512

Enumerated

   

STORED_EVENT_ENABLE

   

X

4306

BitString

   

TRUNK_NUMBER

   

X

549

Unsigned

   

USER_NAME

   

X

2390

Character String

X

 

USER_SELECTED_STATES_TEXT

   

X

1103

Boolean

X

 
1 For N2 integrations, the range is 2-16.
2 Only writable when Out of Service is set to True.
3 Only present when the instance supports intrinsic alarming.
4 Only writable when EVENT_DETECTION_ENABLE is present and is True.
5 Not present in all instances.