Product Description - Metasys - LIT-12013310 - Server - Open Application Server - 12.0

Open Application Server (OAS) Protocol Implementation Conformance Statement

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013310
Version
12.0
Revision date
2022-07-06
Product status
Active

The OAS is a component of the Metasys system. In terms of the BACnet protocol, the OAS is BACnet Testing Laboratory (BTL) listed and certified to the BACnet Building Controller (B-BC) profile and to the BACnet Secure Connect Hub (B-SCHUB) profile.

The OAS can display data from and edit values across a network of BACnet devices. An operator views the data on a web browser that is logged on to the web-enabled user interface of an OAS.