Networking Options - Metasys - LIT-12013310 - Server - Open Application Server - 12.0

Open Application Server (OAS) Protocol Implementation Conformance Statement

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013310
Version
12.0
Revision date
2022-07-06
Product status
Active

Router, Clause 6: None

   

Annex H, BACnet Tunneling Router over IP

   

BACnet/IP Broadcast Management Device (BBMD)

   
 

Does the BBMD support registrations by Foreign Devices?

Yes

No

 

Does the BBMD support network address translation?

Yes

No

Note: The NAE8500 series device cannot be used as a router.