BACnet Secure Connect Node
If direct connections are supported:
OAS without integrations
Maximum number of simultaneous direct connections initiated: 200
Maximum number of simultaneous direct connections accepted: 200
OAS with integrations
Maximum number of simultaneous direct connections initiated: 150
Maximum number of simultaneous direct connections accepted: 150
BACnet Secure Connect Hub Function
OAS without integrations
Maximum number of simultaneous hub connections accepted: 200OAS with integrations
Maximum number of simultaneous hub connections accepted: 150
Additional cipher suites supported beyond
those required for TLS V1.3
The additional cipher suites supported using the cipher suite names as of the TLS Cipher Suite Registry at IANA (See RFC 8446):
____________________________________________________________________
Additional Transport
Layer Security versions other than V1.3 supported
The TLS versions other than V1.3 that are supported, including the supported cipher suites for the version beyond those required, using the cipher suite names as defined by the TLS version supported:
________________________________________________________________________
Generates private keys internally, and
provides matching certificate signing requests.
DNS host name
resolution supported (RFC 1123)