The Metasys UI is a HTML5-compliant web interface that provides access to Metasys from smartphones, tablets, and computers. The Metasys UI is an intuitive interface that reduces learning time, maximizes productivity of operators, and provides a seamless user experience no matter what type of client device is used to access the system. The client device does not require any additional software installation—no Java™, Microsoft Silverlight®, Adobe® Flash®, or other software from an online app store. The Metasys UI is included with the OAS. For more information about Metasys UI, refer to the Metasys UI Help (LIT-12011953) and the Metasys UI Technical Bulletin (LIT-12012115) .